alnx512.Z and alnx609.Z are Linux drivers

alnx512.Z is used for kernel version 2.2.x and 2.4.x system.
alnx609.Z is used for kernel version 2.4.x and 2.6.x system.

Copy the appropriet file to a Linux system and uncompress it to get original diskette copy. You can then create a driver disk. This is what you should do:
 
#mcopy a:alnx512.Z
#uncompress alnx512.Z
#dd if=alnx512 of=/dev/fd0